Title

Essayez la recherche par mots-clés, réf. de commande / code produit ou numéro de série, p. ex. "CM442" ou "Information technique"
Entrez au moins 2 caractères pour démarrer la recherche.
  • Historique

Circular economy in process industries: Rethinking resources sustainably

Advancing circular value chains through efficient processes, reliable measurement and greater transparency

Experts for sustainability initiatives in front of a biogas plant
From linear to circular

Moving from linear consumption to circular value

Traditional linear models follow a "take, make, dispose" approach. Circular economy principles seek to retain the value of materials and resources for longer through efficient use, reuse, recovery and closed-loop approaches.

For manufacturers, this requires considering resource use throughout the lifecycle, from raw materials and production to reuse and recovery.

Productive use of resources

Keeping resources in productive use

Circular manufacturing starts with understanding how resources move through processes and where value can be retained. More efficient production, longer lifecycles and the reuse of suitable materials and process outputs can help reduce dependence on virgin resources while supporting more resilient operations.

  • Use resources efficiently: Identify unnecessary material, water and energy losses and improve the efficiency of industrial processes
  • Extend useful life: Support approaches that keep products, components and assets in productive use for longer.
  • Recover and recirculate: Return suitable materials, water and process outputs to production or other productive uses.
Circular economy wheel: From product design and production to recycling ©Endress+Hauser
Processes & value chains

Circular manufacturing connects processes and value chains

Circularity often extends beyond an individual process or facility. Secondary materials, reusable process outputs and recovered resources can move between processes, sites and organizations.

Closed-loop approaches and collaboration across value chains can create opportunities to retain resource value and reduce demand for additional raw materials. Reliable information about the quality, quantity and characteristics of these resources can support decisions about their potential reuse.

Water reuse

Keep water in circulation

Treating and reusing water can reduce demand for freshwater resources, reduce dependencies and support more resilient industrial water cycles.

Traitement avancé des eaux usées pour la réutilisation

La hausse de la réutilisation de l'eau est encouragée par des méthodes de traitement innovantes, sûres et de plus en plus rentables. 

Plus d'infos

Aborder les enjeux mondiaux de l'eau exige des réglementations sécurisées et des solutions innovantes de réutilisation de l'eau

Aborder les enjeux mondiaux liés à l'eau exige des cadres réglementaires sécurisés qui adoptent les solutions innovantes de réutilisation de l'eau.

Plus d'infos

Réutilisation des eaux municipales et industrielles

Pour lutter contre la pénurie d'eau, les municipalités et les industries adoptent de plus en plus les pratiques de réutilisation de l'eau. Les progrès technologiques constituent la base pour le traitement sûr et fiable des eaux usées.

Plus d'infos

Gestion des risques de la réutilisation de l'eau

La réutilisation directe et indirecte de l'eau potable est une pratique connue, mais la compréhension des risques associés est essentielle à la protection de la santé humaine et environnementale.

Plus d'infos

Assurer la qualité de l'eau avec la filtration sur membrane

L'instrumentation de process dans la filtration sur membrane joue un rôle crucial pour assurer la qualité de l'eau. Le défi opérationnel est d'éviter l'encrassement, le blocage et l'endommagement des membranes.

Plus d'infos

Stratégies de protection de l'eau pour la durabilité

Du fait de la pénurie mondiale d'eau, il est nécessaire que les utilisateurs privés et industriels adoptent des méthodes viables pour réduire la consommation de cette ressource essentielle.

Plus d'infos

Circular and bio-based resources

Create value from alternative resources

Biocarburants durables : montée en échelle pour une économie circulaire efficace

Découvrez comment les biocarburants durables transforment les matières premières renouvelables et les flux de déchets en valeur, contribuant ainsi aux objectifs d'économie circulaire, à la réduction du carbone et à une meilleure utilisation des ressources.

Plus d'infos

Produits biochimiques et économie circulaire : optimiser la chaîne de valeur biologique

Découvrez plus en détail les principaux moteurs, la pression réglementaire et les défis des process qui façonnent la chaîne de valeur biologique dans la production biochimique

Plus d'infos

Production de biogaz et de biométhane à partir des boues et déchets

Des déchets aux flux d'énergie utilisables : découvrez comment la production de biogaz et de biométhane combine la digestion, l'épuration et un fonctionnement stable pour contribuer à une gestion circulaire des ressources.

Plus d'infos

Waste management

Recover value from unavoidable waste

Preventing waste and keeping resources in productive use remain central to a circular economy. When waste cannot be avoided or directly reused, effective waste management can help recover remaining material or energy value and manage residual materials responsibly.

Waste management therefore complements circular economy strategies by addressing resources once prevention and direct reuse are no longer possible.

Les process et technologies de gestion des déchets, moteurs des progrès de l'économie circulaire

Une gestion efficace des déchets est essentielle pour le développement durable, la conformité réglementaire et la réussite de l'entreprise.

Plus d'infos

L'incinération des déchets consiste à transformer les déchets non recyclables en une source d'énergie fiable

Le traitement thermique des déchets joue un rôle important dans la gestion moderne des déchets, car il réduit considérablement leur volume, produit une énergie renouvelable fiable et élimine les polluants du cycle des nutriments.

Plus d'infos

Process transparency

Measurement brings transparency to circular processes

Circular improvements depend on knowing how resources move through production. Reliable measurement and process data help provide visibility into inputs, outputs and losses and identify where resources can be used more efficiently. This transparency can support manufacturers in:

  • Identifying resource losses and efficiency opportunities
  • Monitoring material and resource flows
  • Optimizing processes for reuse and recovery
  • Evaluating improvements using reliable operational data

Measurement therefore connects circular economy ambitions with day-to-day industrial operations.

Measurable progress

Turn circular ambitions into measurable progress

Circular economy initiatives become more actionable when resource flows and improvements are transparent. Relevant indicators depend on the process and application and can include resource consumption, material losses, secondary inputs, recovered outputs and water or energy use.

  • Understand resource flows: Establish transparency around resource inputs, outputs and losses.
  • Improve resource efficiency: Identify opportunities to reduce consumption, prevent losses and increase reuse or recovery.
  • Verify progress: Use reliable operational data to understand whether improvements are delivering the intended results.

Building a more circular industrial future

The transition toward a circular economy goes beyond better end-of-life management. It starts with using resources efficiently, preventing unnecessary losses and identifying opportunities to keep materials, water and other resources in productive use.

Reliable measurement, efficient processes and collaboration across value chains can help manufacturers turn circular economy principles into practical improvements and strengthen resource resilience.

FAQ

Everything you need to know about circular economy in process industries and manufacturing

Notes finale

Looking for more?